Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Product List
SAM9M10-Slide4

This slide illustrates the pipeline mode, in which the post processing engine has to be combined with the hardware decoder. The video or the JPEG image will be decoded using the hardware decoder and then processed using the post processing engine, configured in pipelined mode to display the rendered video or the decoded image. The table shown on the bottom of the slide summarizes the different input and output data formats supported, and the minimum and maximum image sizes in input and in ouput.

PTM Published on: 2011-08-22