Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Product List
SAM9M10-Slide8

As shown on this slide, Picture in Picture (PiP) allows the free positioning of the output image inside the video memory, enabling features such as a channel preview in the active video area. Another feature is the masking feature, two separately programmable rectangular areas of scalable size and position which are blocked from refreshing. The user interface does not have to be redrawn for every frame, resulting in a simpler implementation and performance gain.

PTM Published on: 2011-08-22