Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Product List
summary
In summary, the Microchip SAM9M10 hardware video decoder is capable of decoding video up to D1 (720 x 576) and WVGA (800 x 480) resolution. It can decode multiple profiles, although some are with resolution or frame rate restrictions. The SAM9M10 is also capable of decoding JPEG images, in the sequential DCT-based compression mode which supports the JFIF image file format.
PTM Published on: 2011-08-22