Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Product List
capable of decoding
The SAM9M10 Hardware Video Decoder is capable of decoding videos up to 720 x 576 (or 800 x 480) resolution at 30 frames per second for the following CODECs: MPEG-1, MPEG-2, MPEG-4, H.263, H.264 and VC-1. It also embeds a JPEG decoder which supports JPEG/JFIF file format which is the most common format for storing and transmitting photographic images on the Web.
PTM Published on: 2011-08-22