Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Product List
h.264
H.264 is a highly efficient codec designed to produce better quality at substantially lower bitrates than older codecs such as MPEG-2 or MPEG-4. This is the most popular web video CODEC supported by the latest verisons of Quicktime, Flash or DivX player, and is the preferred video CODEC of the Blu-Ray disc. VC-1 also is a highly efficient CODEC which targets the same applications as H.264 but which focuses more on Microsoft World as this is their primary video CODEC. This is, for example, the XBOX 360 video CODEC and also one of the CODECs supported by Windows Media Player. The Microchip SAM9M10 also supports these two video CODECs which introduce high definition for video.
PTM Published on: 2011-08-22