Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Product List
supporting a level
However, the user has to take care of the following: supporting a level does not mean supporting all resolutions and frame rates defined in that level. For MPEG-2, the SAM9M10 supports all Main Profile levels as previously described, but at a maximum resolution of 720 x 576 and at 30 frame rates max per second. It can be seen in the right hand table on this slide that if the High Level is supported, the maximum defined resolution for that level, 1920 x 1152, is not. This is because the SAM9M10 Video CODEC has a maximum resolution of 720 x 576 at 30 fps. This does not prevent the SAM9M10 from supporting the level, but it does so with some restrictions.
PTM Published on: 2011-08-22